4/25/2016 6:17 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35925 Rating:
|
Since you have the enable input (EN) with have a fixed HIGH signal connected, only one entry is created (1 line). To create a line, an edge from low to high are detected. Between two edges a minimum pause time of 500 ms must be. If the pause times shorter, all edges are ignored within 500 ms, it is not entered. AttachmentLOGO! 8 Soft manual 0BA8 2014_06 sides 253-254 (data log).pdf (251 Downloads) |
4/27/2016 1:19 AM | |
Posts: 124 Rating:
|
Thank you again. |
4/27/2016 5:33 AM |
|
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35925 Rating:
|
For thanks there is a button "To thank" under every post. |
Follow us on