1/26/2010 10:34 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Ok guys, What do you prefer when creating CFC charts: I have to engineer a silo control system, where six silo's can be selected to be filled and emptied in auto and manual mode. I have a SCL source for filling and empting, MEAS_MON blocks to check the silo's for their level, and different OP_D blocks to control the silo's manually. One silo has three sensors: high level, low level and high high level. In total 6x3 = 18 MEAS_MON blocks. How do you guys program this? I create one CFC chart named: MEAS_SILO_LEVEL and in sheet 1, I put the three sensors ofsilo 1and in sheet 2 , I put three sensors fromsilo 2 and so on. I can also create one CFC chart for every silo. Grtzzz So what do you prefer |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on