1/4/2022 6:57 PM | |
Posts: 257 Rating:
|
Hello SIOS Forum Community, We are often asked whether it is possible to mix the SIPLUS modules and the Standard modules of the ET 200SP or the ET 200MP in one configuration. It is possible to mix these modules in one configuration, but the motto applies: "The chain is only as strong as its weakest link". The decentralised periphery should only be used in the environmental conditions that are also approved for the standard modules of the ET 200SP or the ET 200MP. The following can be helpful for configuring the decentralised periphery: Best regards, SIMATIC International Technical Support Hub |
Follow us on