1/31/2022 12:28 PM | |
Joined: 12/28/2016 Last visit: 11/12/2024 Posts: 364 Rating:
|
I have been testing ET200Pro I/O (AI,DI,DO) Initially all Modules show SF but once the Master is connected only the Slot4 Module stays in SF
IF the Module showing SF is removed and updating the configuration rest of the modules are OK Does it mean this module is faulty Please see pictures also. I have a same part# Module and when the faulty one is used the SF led comes on , on replacing it with the other module which has same part # the SF LED goes away and also BF goes away. AttachmentET200pro.zip (514 Downloads) |
Last edited by: qwemx at: 01/31/2022 12:30:21Last edited by: qwemx at: 01/31/2022 12:34:24Last edited by: qwemx at: 01/31/2022 12:34:44Last edited by: qwemx at: 01/31/2022 12:35:19With kind regards... |
|
Follow us on