4/2/2012 3:06 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello SudhirS, GD Communication is not Possible through PLCSIM, but you can used the SFB14 & 15 GET & PUT Block for MPI Communication You will find the Below link Which components are not supported by S7-PLCSIM V5.4 SP4? You can download the latest Service pack from the Below link Service Pack 5 incl. Update 1 for S7-PLCSIM V5.4 |
Ammy |
|
This contribution was helpful to
1 thankful Users |
4/3/2012 9:39 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello SudhirS, Have a look on the Below Link, with X_PUT & X_GET you don't need to download the Hardware in to both CPU, How does data communication work between S7-300/S7- 400 and S7-200 via MPI using S7 basic communication? in Above like it is for S7-300/400 with S7-200 but you can used the S7-300/400 on other hand. it is very easy & you can change the data Length at any point within Defined limit. |
Ammy |
|
Follow us on