11/9/2016 7:22 AM | |
Joined: 3/28/2015 Last visit: 8/15/2025 Posts: 725 Rating:
|
Hello, Kindly have a look at the following points: 1-How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs?It is not possible for users to format a SIMATIC Micro Memory Card (MMC). All you can do is "reset" an MMC, which deletes all user data. 2-Why is the MMC no longer recognized by SIMATIC devices after it has been formatted in a third-party device?If an MMC of the S7-300 is used for non-SIMATIC purposes or is formatted in a third-party device, then the internal structure of the MMC is overwritten and cannot be restored. In this the SIMATIC CPU no longer recognizes/accepts the MMC. It is then no longer possible to use this MMC in a SIMATIC CPU. 3-Which devices can you use to read from, write to or delete from an S7-300 MMC (Micro Memory Card) outside the CPU?The SIMATIC Micro Memory Cards (MMCs) of the S7-300 may be read or written only by the following devices outside the CPU:
|
Eng.Mohamed Ibrahim |
|
11/9/2016 7:44 AM | |
Posts: 15 Rating:
|
so there is no hope to restore it |
11/9/2016 7:46 AM | |
Joined: 5/12/2006 Last visit: 9/1/2025 Posts: 22709 Rating:
|
correct! |
11/10/2016 3:57 PM | |
Posts: 15 Rating:
|
thanks very much i solve the problem |
Follow us on