6/23/2012 4:51 PM | |
Posts: 378 Rating:
|
Dear All, As I have seen catalogues, brochures and forums about MP377, it says it is open platform and possible to add custom AxtiveX components like .ocx , .dll . When I tried to add ActiveX components to WinCC Flexible advanced version using the device type as WinCC flexible runtime, I can find “My Controls” tab under “Tools” bar. Then I can add any of my ActiveX components. But when I choose device type MP377 I can not find “My Controls” tab under “Tools” bar. The only tabs showed are “Simple Objects” , “Enhanced Objects” , “Graphics” and “Library”. I have attached here the snapshot pictures of the above two trials. I don’t know how but I am sure of that it is possible to insert any ActiveX component on MP377 by some means because Media Player is appeared under “Enhanced Objects” . My question is how to insert an ActiveX component to MP377? Note that I have searched a lot of threads on this forum regarding this but all of them couldn’t answer my question. AttachmentMP377 ActiveX.zip (342 Downloads) |
6/24/2012 2:14 PM | |
Posts: 378 Rating:
|
Help help help....... |
6/25/2012 10:12 AM | |
Posts: 3037 Rating:
|
Hello, You can find more information in the following link. How do you register an ActiveX object on the configuration computer and then incorporate it in WinCC flexible? Tweety |
6/25/2012 2:39 PM | |
Posts: 378 Rating:
|
Sorry I already seen and understood the link(I already attached the screenshoots for my trials) The information on the link is applied for WinCC Flexible runtime device, NOT for MP377. If anyone done for MP377 please please and please tell me the steps and attach the screenshoots. Thanks |
8/10/2012 2:31 PM | |
Posts: 378 Rating:
|
Still waiting for some one |
Last edited by: desmul24 at: 8/10/2012 2:38 PM |
|
8/13/2012 11:51 AM | |
Posts: 3037 Rating:
|
Hello, Perhaps you getmore information about ActiveXhere. Is there a Siemens contact for customer-specific software solutions, extensions to WinCC flexible or own applications for Windows CE Panels? Tweety |
1/7/2022 3:10 AM | |
Joined: 2/14/2020 Last visit: 1/25/2024 Posts: 24 Rating:
|
have a look at yzx-tia-additionalcontrols |
Follow us on