3/21/2022 11:41 AM | |
Joined: 3/21/2022 Last visit: 3/23/2022 Posts: 4 Rating:
|
Hello All, I am still new to the Siemens logo and I am building my first program for a conveyor. I managed to work the conveyor through the PLC. Now my task is to add the start, stop and also a reset. The reset button will be there so when the emergency is pressed and then released will home all the positions. Now I need to add these three functions to the program. Additionaly, I am attaching my program of what I have done until now. Attachmentpart1_and_2_15022022_withpistionupddate.zip (337 Downloads) |
Follow us on