4/12/2010 3:38 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hello, currently I have problems with Wincc. Script errors, cannot activate/deactivate.... When I started with PCS7, I installed on my ES the complete package of PCS7. That is: choosing "User defined installation" and installed everything except for the trial license Now I was wondering (because I've read documents) if this can cause me the problems... I'm using the ES as ES/OS so engineering and process control. Or did I have to choose for "Package installation" and choose the components under: Engineering (PCS7 engineering, Batch engineering, Routecontrol engineering, PDM) Big mistake?! |
If I could help you, you can use the RATE button. Thank you. |
|
4/12/2010 4:59 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Yeah, maybe better. PCS7 installed correctly but have some weird errors. Maybe because I installed everything or/and because I didn't have an english(read as MUI)XP install, so a lot of diagnose files in the winccproj are in my own language, not in english. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on