2/22/2022 7:27 AM | |
Posts: 1 Rating:
|
Salve gradirei capire come procedere per aggiornare logo 8 fw version 1.82.02 |
2/22/2022 7:35 AM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
Hello menny73, at first welcome to the forum. This is a english speaking forum. Please be so kind and write your next posts in english.
You can only update from FW V1.82.02 to V1.82.04. You need a FAT32 formatted mSD card. The FW update can you download from here: Product information on the firmware update for LOGO! 8 for security Vulnerability CVE-2020-7593Upgrading the firmware for LOGO! V8.2 FS:01/FS:02 Download the firmware update file, decompress and save it on your the PC. Back up the user program in LOGO! BM to your PC. Copy the three firmware update files to the root directory of the Micro-SD card. Note: Don’t change anything of the firmware update files, for example, the file name. Otherwise LOGO! BM may not complete the firmware upgrading. Switch off the power supply for LOGO! BM. Insert the Micro-SD card in LOGO! BM. Switch on the power supply for LOGO! BM. Make sure that the power supply is stable during the entire firmware upgrading process and within the permissible range described in the LOGO! System manual. Check the firmware version in the LOGO! BM after the firmware upgrading. Check the user program, function and settings in LOGO! BM and adapt them if necessary.
|
Follow us on