11/19/2009 3:42 PM | |
Joined: 9/29/2005 Last visit: 7/16/2025 Posts: 313 Rating:
|
Dear JoanR,
i am wondering from where you get your project?! Within the Micro Automation Set 5 the library-blocks are called SMS_init,-send,-receive, .... Furthermore the Errornumber "512" is not well-known to me. Can you tell me, where you downloaded this project?
Because of this i guess you are using a old version of Micro Automation Set 21 where the new MAS5-SMS-library is not yet included. Till you send me your project i cannot say anything to your described errors. But i suggest you anyway to use the most actual Micro Automation Set 21 - Version with the most actual MAS5-Version included. The only thing i can imagine with your description is that your address of the variable with the content "Hello" is violated by any other variable. But anyway: Tell me if you are willing to use the new Micro Automation Set 21, or please attach your current project here. regards Lif |
Follow us on