7/24/2014 5:05 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
You should use external pre charge circuit using resistors. Make logic such that, DC voltage will applied through resistors first and after getting some voltage - 80%, switch to main contactor. This will help you to avoid fuse failures Now- as far as spares concern, you can find fuse part no from catalog and manual as well catalog & in Manual Inverter (DC-AC) Compact Type Inverter (DC-AC) Chassis Type Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
1 thankful Users |
7/28/2014 7:24 AM | |
Posts: 11 Rating:
|
Thanks got Fuse chart. Regards, Pralhad |
Follow us on