8/21/2014 8:09 AM | |
Posts: 2 Rating:
|
Dear all, We've changed a motor which has different torque and current. I tried to change torque P113 and current P108 and made parametr. at standstill P115=2.After that motor started work with highest torque( this is question why ? ) and accordingly we werelimited by rpm's ( this is understandable ).Because we strongly needed more rpm's, I changed back torque,and everythingworked correctly, but with different torque, than in motor plate. I would like ask a question: There is parameters P354,P353,P350- torque,rpm and current. What's difference from P113 and P108. Do I need change these both parameters, when I changing torque and rpm's. I thought, that P354, P353 will automatically adjust, when initialisation P115=2 will be made, but that's not true. I'm using 6SE7032-1EG60, motor 90kW. Parameters pdf list added. Please, help to solve that problem. Thanks a lot
AttachmentNr1.pdf (405 Downloads) |
Follow us on