10/18/2016 2:29 AM | |
Posts: 124 Rating:
|
Hello, I have a doubt about inserting parameters in the message area, specifally inserting <Time Base>. The time base can be set to h, m, s and ms. When inserting a time base parameter from a function block in the message area, its rectangle takes seven cells. After, trying to insert another parameter, like <Current time> it is not possible to superpose partially the new over the first. Result: six cells will be free between Current time and Time Base. (five free cells for ms time base). A shot screen illustrates this case. Some help? Regards, AttachmentMessage text issue 18 10 2016.zip (176 Downloads) |
10/18/2016 6:14 AM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
The real problem is that the LOGO! 0BA8 Display analog values left-aligned. In addition, in your case the stopwatch is a special case. The current time is not displayed in time format, but as a number with the base of the time base used. 2m30s are not displayed as 02:30, but as 90 when the time base is seconds. You can use the "Scale time" function. See attachment. AttachmentScale_time.zip (186 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on