7/13/2015 11:52 AM | |
Posts: 35 Rating:
|
Hello, I am using two MasterDrive MC with resolver feedback one for Conveyor as Master and other for Piston. Using F01 technology Conveyor drive run as control mode and Piston drive as Synchronous mode with CAM profile. In CAM profile upper limit is 985 LU and Lower limit is -2217 LU of piston according to the Conveyor position. I run the system at low speed piston works perfect as system speed increases upper and lower limit of piston reduce according to speed (i.e 10% of Master piston limits 985 & -2217, 100% of Master Piston limits 580 & -1439) Kindly solve this issue. I attached both drives file. Attachmentforum.rar (354 Downloads) |
Follow us on