7/1/2011 12:10 PM | |
Joined: 8/16/2010 Last visit: 7/8/2024 Posts: 50 Rating:
|
Hello, [schnippschnapp] My next problem (and maybe this should go in a new thread) is that the MP177 (6AV6652-2JC01-2AA0) doesn't appear in the TIA V11 device configuration list, although it is listed in the supported hardware. Do I need to update the device listing and if so how Thanks for all the advice, RandomCoder Splitted from Alternative for S7-400. |
Last edited by: O_Moderator at: 7/1/2011 12:27 PMnew subject after splitting |
|
7/1/2011 3:17 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear RandomCoder, Can you tell which version of WinCC v11 you have? (WinCC v11 Basic, Comfort, etc) Delivery release SIMATIC WinCC V11 Best regards, Wizard |
7/6/2011 4:33 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear Robster, The reason you can not find the mentioned MP177 (6AV6 652-2JC01-2AA0) is because it is a combination of WinAC MP and MP177 See this link: http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6AV66522JC012AA0&caller=view So that is the reason you can not find it. Best regards, Wizard |
7/8/2011 10:53 AM | |
Joined: 5/28/2008 Last visit: 9/5/2025 Posts: 1344 Rating:
|
Thanks. But then RandomCoderwill also do not find it and his problem is not solved. |
Follow us on