1/20/2022 9:27 AM | |
Joined: 4/26/2014 Last visit: 4/29/2024 Posts: 26 Rating:
|
Hi, Can someone pls help me to find the GSD file for this particular slave device, attached file? WAGO 750-343, B757_V10.gsd thank you so much
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2022 12:59:45New subject after splitting |
|
1/20/2022 1:05 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi jruz1, have a look on the WAGO-page: https://www.wago.com/de/io-systeme/feldbuskoppler-profibus-dp/p/750-343#downloads hope this helps, regards, |
FCK WAR! |
|
1/21/2022 5:16 AM | |
Joined: 4/26/2014 Last visit: 4/29/2024 Posts: 26 Rating:
|
Hello everybody, I am the same guy of this post, and the main issue is to add CP card which happens to have a RIOs on the Controller setup which is WAGO. I dont have access to the old project file, or to the programming terminal, this has been there 10years ago. Inquiry about adding CP Card - Entries - Forum - Industry Support - Siemens |
1/22/2022 5:39 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello jruz; I agree that looking for a very old file can be very frustrating at times. The B757_V10.GSD that you are looking for is no longer provided by Wago downloads. One of my interesting ressources for gsd files is the GSD-DB.com Profibus gsd database, that I often refer to for general information . unfortunately, the site does not seem to be active right now, so registration and downloads are not enabled (for the moment, I hope). But doing a search for the B757_V10.GSD in the GSD-DB site only provides the results you see in the following attachment. Note that each of these distinct gsd file refers to a specific version of firmmware of the 750-343 Profibus coupler. In my experience, if it is not in the GSD-DB database, it must be a very old file that only the manufacturer could provide. http://www.gsd-db.org/index.php?keyword= When you contact Wago for support, make sure provide them with the firmware information that is oin thetext box at the bottom of the module front bezel, that would be an important information for the search by Wago techs. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/22/2022 17:40:34Last edited by: dchartier at: 01/22/2022 19:59:20Last edited by: dchartier at: 01/22/2022 20:10:09 |
|
1/24/2022 12:49 AM | |
Joined: 4/26/2014 Last visit: 4/29/2024 Posts: 26 Rating:
|
Thanks Daniel for the info. Yes, I cannot even see on this site GSD-DB as you did. Unfortunately, I am not registered on this site, I am not receiving an email from them to confirm my registration. I already sent an email too on WAGO support, until now they haven't responded to me. Im just hoping now that the someone may have the file, while waiting for WAGOs support. Thanks again. Regards, |
Follow us on