9/26/2017 7:38 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
The analogue input of the LOGO! generally reads a current signal as 0-20 mA (or a voltage signal as 0-10V) and converts it into 1000 units. This results in:
AttachmentLogo overview analog voltage current units.pdf (535 Downloads) |
Last edited by: ixo65 at: 9/26/2017 7:43:21 PM |
|
This contribution was helpful to
1 thankful Users |
9/28/2017 9:26 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
If you want to parameterize a 4-20 mA sensor in the analog amplifier, you do not need to calculate anything, this makes the LOGO! Software automaticly. You only have to select the sensor type 4-20 mA for the amplifier, then enter the upper (maximum) and lower (minimum) limits of the measurement range and the number of decimal places. The software then automatically calculates the parameters gain and offset independently. Example: 4-20 mA sensor with a measurement range from -30 bar to 90 bar, displaying with one decimal place. Type of sensor: 4-20 mA The software calculates a gain of 1.5 and an offset of -600. AttachmentTest.zip (395 Downloads) |
Last edited by: ixo65 at: 9/28/2017 9:28:59 AMAttachment |
|
This contribution was helpful to
1 thankful Users |
9/28/2017 4:59 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
You could also calculate the gain and the offset itself. Example again the sensor with the data: This would require an extended measuring range for a sensor with 0-20 mA if a measured value of -30 bar is to be displayed at 4 mA.
AttachmentTest_0BA8.Standard.zip (354 Downloads) |
Last edited by: ixo65 at: 9/28/2017 5:24:42 PM |
|
This contribution was helpful to
1 thankful Users |
9/28/2017 6:48 PM | |
Joined: 2/24/2017 Last visit: 12/9/2022 Posts: 33 Rating:
|
very helpful thanks |
This contribution was helpful to
1 thankful Users |
Follow us on