7/22/2022 3:59 AM | |
Joined: 2/24/2016 Last visit: 3/10/2025 Posts: 1 Rating:
|
Hello, We are communicating to a PAC3220 with ModbusTCP and have found that we can read the THD-V (Y) when the device is in 3P4W mode, but we cannot read the THD-V(delta) in 3P3W mode as it is not in the Modbus map, and the THD-V (Y) becomes "-nan". From the manual (see attachment) the THD-V L1..L3 is only available in 3P4W mode, but THD-V L1-L2, L2-L3, and L3-L1 is available in 3P3W mode. Has anyone been able to read the phase to phase THD-V over modbus? It is reading on the meter. Thanks in advance, David. AttachmentPAC3220 Manual information.pdf (795 Downloads) |
Follow us on