7/6/2010 2:43 PM | |
Posts: 325 Rating:
|
Dear all, We have commissioned PCS7 V7.1 project and its been working well since last 2 months. Meanwhile the client has done few changes inAS & OS,and since then we got this perticular problem. All Block Icons and Objects ( like Bar Graphs )blink continuously. This happens for all the Block Icons and Bar Graphs in each & every Graphic File. In attachment is the video clip where in one can see the blink happening. Can any one help me with this issue!!! Rgds Nil AttachmentP6180120(00h01m41s-00h01m52s).zip (148 Downloads) |
Last edited by: O_Moderator at: 7/6/2010 2:49 PM |
|
7/7/2010 8:28 AM | |
Posts: 183 Rating:
|
Hello Nil96; Did you try change to wincc classic. The behavior is the same? |
7/7/2010 9:03 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
I think it has something to do with the read/write of the tags...because the icon is only blinking when the value changes... Because all icons are blinking, it has to be a general problem. So like CBO said, you should check the scripts. What happens if you set theupdate cycle time to a different value. If it is on user defined, select a standard one, like 1 or 2 sec. Maybe you could try to copya standard CNTRL_PID block icon from the @@PCS7typcials file to your @PCS7typicals file. (Save your custom icon first). Assuming your are using a CNTRL_PID as seen in the movieclip... |
If I could help you, you can use the RATE button. Thank you. |
|
7/7/2010 10:47 AM | |
Posts: 325 Rating:
|
Hi Cbo & Oreca, Thanx for ur reply. Infact there are 3 scipts for the entire project. These are untouched... Rgds Nil |
Follow us on