6/4/2013 11:49 AM | |
Joined: 6/4/2013 Last visit: 7/1/2015 Posts: 4 Rating:
|
Introduction: This is a S120 application on Vibration welding machine. Friction welding(FRW) is a class of solid-stateweldingprocesses that generates heat through mechanical friction between a moving workpiece and a stationary component, with the addition of a lateral force called "upset" to plastically displace and fuse the materials. My problem is, the load current fluctuates sharply in stable state. How I could control the current and make it fluctuate smoothly? Meanwhile, The Lenze 9326 uses for this type of machine, load current fluctuates ±1A according to the setpoint. Configuration Drive: S120 / CU310 DP: 6SL3040-0LA00-0AA1 PM340: 6SL3210-1SE22-5UA0 TM31: 6SL3055-0AA00-3AA1 25.50 A/ 11.00 kw Load side are two electromagnets, the parameter is Max current: 35.2a Vol: 900v Max feq: 130hz Power: 13.75kw Rated : 25A More details including structure charts and trace could be seen in attachment. AttachmentD:\introduction_en.pdf (120 Downloads) |
7/5/2013 11:25 AM | |
Joined: 6/4/2013 Last visit: 7/1/2015 Posts: 4 Rating:
|
Dear experts, would you please give me some advice? Thank you very much. |
Follow us on