1/23/2025 2:25 PM | |
Joined: 3/10/2023 Last visit: 4/14/2025 Posts: 3 Rating:
|
Hello, I have B&R soft PLC communicating with the S120 drive. The machine is using the a synchronous motor and technology Controller. The parameters are send using Profibus. Currently the PID gains are programmed as value for the below parameters.
Is it possible to send these parameters from PLC? or not? If yes what is the procedure? I have uploaded the parameters text file for the S120 and config files. Attachmentpara.txt (81 Downloads) |
Last edited by: AutoGen_1979044 at: 01/27/2025 06:53:44 |
|
Follow us on