5/17/2012 12:19 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, i found important FAQ for checking in-house logic stuff on PLCSIM with some updated features. Please check it out. How do you simulate communication between two CPU modules? Which components are not supported by S7-PLCSIM V5.4 SP4? Where can you find information on the topic of "Loading and testing S7 programs"? How can you use the "Record/Playback" function in S7-PLCSIM to record a sequence of events? How can you switch between an S7 CPU and an S7 PLCSIM? How do you test the I/O using the S7-PLCSIM simulation program? How can you operate S7-PLCSIM (RUN-P, RUN, STOP and MRES) directly from WinCC Runtime? Hope this will helps. |
VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
5/18/2012 7:28 PM | |
Posts: 621 Rating:
|
|
This contribution was helpful to
1 thankful Users |
5/18/2012 7:42 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, But you need PLCSIM V5.4 minimum to work with above features. |
VANDE MATARAM..... |
|
Follow us on