8/24/2017 1:23 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Service Pack 1 (SP1) for LSC V8.1 is available. The SP1 can be downloaded from the side: This is the "Upgrade from LOGO! Soft Comfort: V1.0 / V2.0 / V3.x / V4.0 / V5.0 / V6.x / V7.0 to V8.1 (SP1)". After the download, the file "setup.exe" is available for installation. |
This contribution was helpful to
2 thankful Users |
Follow us on