4/13/2016 4:28 PM | |
Posts: 2 Rating:
|
Hello, currently having problems with a simodrive 611, I am getting EA131 and EA608. I know that they are primarily mechanical bind but I can rotate the assembly by hand freely. It will run for about 4 min then error out. I have tried installing simocomu and connecting rs232 but it won't connect. I have checked p0801 and made sure it was set to zero but still having no luck. I could use some help. I attached the model tag of the drive. Update: I am currently connected with Simucom U by setting my data bits:7, even parity, with 2 stop bits @ 9600 baud. but I notice that my set positon should be 0 but my actual is jumping around +/- 6 degrees? Is that normal for this type of system? I had a spare motor and installed it, it is showing a variation of +/- 5 degrees. Mind you I haven't initiated movement yet, the variation is just while its sitting there in run mode. Also the controller card is a 6SN1118-1NH01-0AA1 ------------------------------------------------------------------------------------------ |
Last edited by: cmyers at: 4/13/2016 4:32:06 PMLast edited by: cmyers at: 4/13/2016 7:41:32 PMLast edited by: CS Moderator at: 09/21/2019 13:24:45New subject after splitting |
|
Follow us on