1/20/2025 10:01 AM | |
Joined: 11/29/2024 Last visit: 2/19/2025 Posts: 1 Rating:
|
Hello everyone, I hope you are all doing well. I'm currently facing an issue with the HMI panels and would appreciate your help. In particular, with the switches on the Comfort panel, there was the possibility to have a button with switch functionality (photo1). However, on the Unified panel, they have been transformed into normal buttons . Does anyone know if there is a way to achieve the same result as in the first photo? I would be very grateful. Thank you in advance for your assistance! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/20/2025 10:19:07New subject after splitting |
|
1/20/2025 10:58 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi rick_ross67, This is not possible by simply configuring a switch as in WinCC Comfort/Advanced. If you want it to look like a button, you have to use a button. For it's event I would recommend to use the InvertBitInTag system function and to change the text according to the tag value you should use a tag dymanization for the text. Kind regards |
Follow us on