10/9/2006 10:24 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Sorry but we need more information from you such as :
Salma |
10/9/2006 11:20 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Hi pranay If you have written a script this implies you are not using the User Archive Editor to save the data. A script runs in runtime and the UA editor is a configuration tool - the two are completely different !! Anyway, if it works on one computer and not another it implies an installation issue. Are you seeing an actual error message anywhere ? The "data not being saved" is a symptom and an error message will help diagnose it. Can you post your Diagnose directory here ? (C:\Program Files\Siemens\WinCC\Diagnose) Also, have you read this thread ? Salma |
10/9/2006 2:29 PM | |
Posts: 3609 Rating:
|
[quote user="pranay"] Hi, I am attaching two files of diagosis of one my HP laptop and other Dell laptop. I have tried with the installation also. But it couldn't work out .I couldn't find any error message. I have read the given thread but as being said in that: user archive-R. It can't be seen in this. Attachmentwincc_diag.zip (153 Downloads) |
10/9/2006 3:20 PM | |
Posts: 69 Rating:
|
Hi, You have a lot of script errors on both PCs. First solve all Your script errors. The following link will help http://support.automation.siemens.com/WW/view/de/22892165 Balu |
11/5/2007 10:59 AM | |
Posts: 25 Rating:
|
Dear Robo.. If your problem is just the "Changes not able to save in the User Archive Editor", Then the following FAQ Will help you. I had a similar problem where the user archive data could not be saved(The save symbol disappears and the Title Bar has a weird -R- Symbol) and the problem was rectified by deleting a Temp file which is explained in the entry below. http://support.automation.siemens.com/WW/view/en/492977 |
Follow us on