9/5/2021 1:14 PM | |
Joined: 7/5/2017 Last visit: 1/1/2025 Posts: 232 Rating:
|
Hi refer attached image Do practical first for voltage varring 1 to 10 v. Measure it on multimeter probe at Vout terminal before connect module. Reference given for v measure. If want measure I then use module pin 9 Uv0 and 13 I0+ of chanel one. Note insure voltage before' connect to module . Module pwr P± and M should there via L bus. Regards Raman S Attachmentvoltage Measure.pdf (640 Downloads) |
Raman |
|
This contribution was helpful to
1 thankful Users |
9/5/2021 10:37 PM | |
Joined: 7/23/2021 Last visit: 1/11/2022 Posts: 20 Rating:
|
Thanks for the insight. So If used a potmeter at 5000ohm, I would need to buy a resistor at 7000ohm? |
Follow us on