1/14/2025 12:08 PM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16386 Rating:
|
Hello LuchianR you can try to reset the runtime files with this and load again to the Panel: https://support.industry.siemens.com/cs/de/en/view/109778709 (I think this will not make it better, but its worth a try) It is normal that you can only select V19.0.0.2 in TIA Portal (there is no newer Device Version available). The newest OS Image for the Panel in V19 is V19.0.0.3 so it is correct if you have installed this on the Panel. (you can also use newer OS IMage versions, in case of WinCC Unified this is possible ((in Comfort/Advanced this was not possible )) Try also with a new Alarm Control does it have the same bugs? If yes then you can also open a Service Request at Siemens Support to check if this is some kind of setting you can adjust or if its a bug Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on