(2)| 10/10/2006 9:43 AM | |
|
Joined: 4/24/2006 Last visit: 1/6/2026 Posts: 9099 Rating:
|
Hello, When you buy a WinCC v6 Runtime License, it's equipped with a Softnet S7 Lean license Best regards, Wizard |
| 10/10/2006 12:30 PM | |
|
Posts: 1398 Rating:
|
Great explanation Reuben ! Yes as Wizard says, Softnet Lean is included when you buy WinCC. See thisFAQfor more information. |
| 10/11/2006 3:20 PM | |
|
Posts: 1275 Rating:
|
[quote user="keyclick"] Our installation is an unlicenced v6.0 Sp4 install... I had tried installing the ill-fated v6 demo DVD, and it failed in the way I have seen others describe on this forum. So our local rep installed a copy, but it is unlicenced. I presume that the Simatic Net is unlicenced, too... I see nothing in the license manager. Should there be any way to confirm if this is present. Does the lean softnet driver work in demo mode at all? (we are trying to evaluate WinCC, and decide if we sould use it...its kinda hard when you cant even connect to a PLC!) Greg, Both WinCC and Simatic Net will work just fine as a demo. The License manager would be showing your licenses, if you had any. If there's nothing there then you're using demo mode for both software. A message box should appear, saying you're in demo mode, but it will not stop either software from working. There should be a problem with your communication configuration. Did you configure the communication card properly? Did you input the IP, rack and slot? About importing the tags have you checked: /tf/WW/en/Posts/4842 Best regards, Danielle |
Last edited by: Danielle at: 10/11/2006 3:22 PM |
|
Follow us on