(0)| 4/1/2007 2:39 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Vido, ForRTyou may look in the handbook: Communication with SIMATIC It is also possible to work with the newest version of the 315PN/DP with Isochrone Profibus DP where you could be use very short and reproducable times on the Profibus. However to use this functions you need V2.5 and this new functions are only working wenn you have STEP7 V5.4 SP1... See also: HOW TO ADD CPU 317 DP/PN v2.5 IN HW CONFIGUREthis is also for the newest V2.5 Firmware for the CPU 315PN (newest version). |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on