(0)| 8/25/2013 1:07 PM | ||||||||
|
Posts: 34 Rating:
|
Dear All please i want your support about configuration in attached system if it is correct or not ? in field layer the communication Protocol ProfiBus In application Layer communication Protocol S7 TCP/IP Hardware ssystem consist of : 1- Redundant CPU :
2- Commonication Processor :
3-Redundant Interface modules in two ET200M :
AttachmentRedundant System S7-400+CPs+ET200M.zip (483 Downloads) |
|||||||
| 8/25/2013 1:13 PM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following threadRedundant System S7-400+CPs+ET200M Best regards O_Moderator
|
Follow us on