6/26/2014 8:41 PM | |
Joined: 3/28/2014 Last visit: 11/14/2023 Posts: 82 Rating: (0) |
Hello Finaly Ive do recommisioning CNC lathe. The owner buy from Germany files needed (%TEA1....) but I suspect that tea1 is original to that machine because the working area was not correct. Exactly I think that they send from smaller similar cnc lathe. I ve change some NC MD data and solve that but I dont know is it necessery to reference toolbox because I have this message at PDF attachment. Especially I'm gratefull to Primotechnics who did giving me advices all the time. Thanks
AttachmentReference.pdf (540 Downloads) |
6/27/2014 1:42 AM | |
Posts: 10 Rating: (1) |
Hi, Thanks, your very welcome! I don't think this i a rel problem you have. The reference points are reached, and the machine should work, correct? Off course it will display a incorrect value when moving the axes to a certain point, but that can be changed. Maybe you should check NC-MD 240*maybe these are set incorrectly? Seethe attached file, maybe that can help. I guess yours is GA3? Gr Bart Attachment338_810_820_GA3_Installation_Instructions.pdf (438 Downloads) |
7/18/2016 12:39 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by Sky Diver840 is split to a separate thread with the subject Sinumerik 810T, download %PCP problem. Best regards |
This contribution was helpful to1 thankful Users |
Follow us on