8/8/2017 9:53 AM | |
Joined: 9/9/2015 Last visit: 9/20/2025 Posts: 732 Rating:
|
Dear All, Anyone of you have SITRANS library for PCS 7 8.2 ? I would like to have the driver block for MAG 6000 and SIPART PS2. Thanks for sharing. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/8/2017 10:03 AM | |
Joined: 9/9/2015 Last visit: 9/20/2025 Posts: 732 Rating:
|
I found the link. Here attached with the download link for SITRANS library. |
Last edited by: JazTai at: 9/7/2017 8:48:18 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
8/8/2017 10:22 AM | |
Joined: 10/26/2011 Last visit: 9/22/2025 Posts: 765 Rating:
|
Thank you for your post and also for the helpful answer. I know this library and I find, that the library is very helpful, if you use the Siemens field devices. You have much more information about the diagnostic and HART variables. |
SIMATIC PCS 7 - Overview |
|
8/9/2017 10:38 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Msc.Automation Eng. is split to a separate thread with the subject Using DP/PA coupler ( AFDiSD) and have Endress devices in the field - How can use SITRAIN library?. Best regards |
9/7/2017 8:36 AM | |
Joined: 9/9/2015 Last visit: 9/20/2025 Posts: 732 Rating:
|
Hi everyone, Here is another small update on SITRANS library V6.0. I encountered a problem with Sitrans Library (link to the post) . After seeking Siemens advices, i found that there are some of the instruments are not compatible with SITRANS library that working in S7 400 Redundant PLC , especially Profibus PA type. Siemens Replied:" The Sitrans Library is only released for single systems. Redundant H-Systems are not supported at the moment from the most profibus pa field devices. The cyclic communication is working well and also the acyclic communication via secondary master e.g.: SIMATIC PDM. Thank you. Hope this is helpful for those who used Sitrans Library in the future. AttachmentDevices_in_the_SITRANS_Library_V6.pdf (172 Downloads) |
Last edited by: JazTai at: 9/7/2017 8:46:12 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
9/8/2017 11:10 AM | |
Posts: 14 Rating:
|
Hi everyone, here you find an application example with the SITRANS Library: Regards Saarlodri |
Follow us on