6/18/2025 10:53 AM | |
Joined: 6/18/2025 Last visit: 6/18/2025 Posts: 1 Rating:
|
This question is regarding configuring PT00 for 6ES7531-7KF00-0AB0. I have connected a 4-wire PT100, 2 wires at pin 3 and 4 and the other 2 wires at pin 7 and 8, according to the module's wiring manual. I have set channel 0 to thermal resistance (4 wire) and standard ranges. All other channels are deactivated. The underflow diagnostics, when enabled, is producing a "low limit violated" error. I have rechecked the sensor wiring and configuration. Is there any error that anyone could point out to, so as to solve the issue? ------------------------------------------------------------------------------------------ |
Last edited by: ria maria_mathew33 at: 06/18/2025 10:54:40Last edited by: Moderator_Lan at: 06/18/2025 10:58:40New subject after splitting |
|
Follow us on