12/24/2017 4:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello dadkhah, Simply loading motor parameter is not sufficient to comission DC drive. Please refer chapter 7 start up of manual (you need to get it download from this link). Just follow the steps from the manuals & carry out optimisation in sequence as mentioned in manual. This will solve your problem. HTH. |
12/28/2017 8:43 PM | |
Joined: 6/21/2014 Last visit: 5/4/2024 Posts: 41 Rating: (0) |
hello and thanks piscaen2010 this is the parameter file of my simoreg . where i mistaked? Attachment6ra70.pdf (300 Downloads) |
12/29/2017 4:50 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello dadkhah, Your drive MLFB is 6RA7031-6DV62. It is 125 A capacity where as your motor rated armature capacity is 20 A & field rated current is 0.2 A. Please set P076.001 = 16%, P076.002 = 2%. Recarry out all optimisations & check. BTW why you are configuring 125A rated capacity drive for such small motor capacity. |
12/29/2017 1:25 PM | |
Joined: 6/21/2014 Last visit: 5/4/2024 Posts: 41 Rating: (0) |
hello yes.You are right. but i test thi drive in workshop . the main program in factory site working with profibus and the own motor. this is the main program that has the same problem. : Attachment6ra70-5968.pdf (259 Downloads) |
1/2/2018 5:06 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Have you checked the set point? How much is it at drive side? |
Follow us on