11/18/2016 5:50 PM | |
Posts: 18 Rating: (0) |
I have 840d ncu Sinumerik connected through MPI Cable with 1)MSTT,MPI-koppl. (MCP) 2) MMC 103'200MHz ,64MB(HMI) mpi 3) VEREYILERBOX (HHU) 4)OPO30 (Magezine) all mpi cable connector switch is in off position except ncu side connector switch, and ncu connected with s7-300 through profibus. I was facing alarm 120202 wait for connection to NC/PLC, i reset the ncu through s3,s4 switches by shifting s3 to1 and s4to2to3for3second and back to 0. After restat i m facing alarm 2001'plc not startup. And archive file are not uploading to ncu. I wish that if someone has the solution then share please. Regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/21/2016 12:53:56 PMNew subject after splitting |
|
11/21/2016 1:50 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
The second thread with the subject 840d ncu, 2001 plc not startup. is located in the SINUMERIK CNC automation systems conference. Best regards |
This contribution was helpful to1 thankful Users |
Follow us on