2/27/2019 11:31 PM | |
Posts: 4 Rating:
|
Hey! I need a help. I am new to handling Analog inputs. I want to make a project in which I would be connecting a Load cell, capacity 450 Kgs, 1-10 Volts, 2 mV/Volt as an Analog Input to Logo. Now, I want like when load goes on 225 Kgs, Logo should give one digital output at Q1. May I have some knowledge about this? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/28/2019 11:05:21 AMNew subject after splitting |
|
2/28/2019 4:23 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
As I have already written to you, you need a corresponding measuring amplifier, which generates from the mV signal of the load cell a 0-10V signal, which the LOGO! then can evaluate. Look at somethings like this: https://www.amazon.com/FidgetFidget-4-20MA-Amplifier-Transmitter-transducer/dp/B07FKXTM8W |
Last edited by: ixo65 at: 2/28/2019 4:30:25 PM |
|
2/28/2019 9:01 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
If the measurement is to be calibrated, SIWAREX is the better solution. |
Follow us on