8/4/2022 6:43 PM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating:
|
Hello, I was able to solve my problem in the following way: 1. As my system has several network cards, I had to edit the hosts file that is in C:\Windows\System32\drivers\etc and there add my different computers with their respective IP address 2. Likewise, I had to give priority to one network card over the other and I did this in the advanced settings of the network card, disabling the automatic metrics function. Once I disabled that function, I placed 1 on the card that I wanted as the main card and placed 2 on the card that I wanted as the secondary card. If you want to know the complete procedure, in my blog (In Spanish) create this step by step in case someone needs it at some point https://instrumcontrol.com/como-asignar-una-tarjeta-de-red-para-compartir-archivos-en-windows/ |
Follow us on