5/24/2016 4:05 PM | |
Joined: 9/8/2015 Last visit: 3/5/2024 Posts: 3 Rating: (0) |
Hello, I have program done in STEP 7 (V5.5 + SP4). It's project that has two CPU's (both are CPU 416F-3 PN/DP) on the same rack (one of them is safety program). Now i would like to upload hardware and software to TIA portal V13 SP1 just to make TP700 screens. But whatever I do, the program does't let me to upload anything. I checked IP addresses, subnet, gateway and it's all good. And if I try to make hardware configuration on my own, it doesn't let me to put two CPU's on the same rack (Is multicomputing possible in TIA V13 SP1?). I also tried with adding new proxy device, that doesn't work too. I did everything like described here: https://support.industry.siemens.com/cs/document/41885693/how-do-you-load-the-project-data-from-the-cpu-into-the-programming-device-in-step-7-(tia-portal)?dti=0&lc=en-WW I get message: "Loading will not be performed because preconditions are not met" and "connect to module CPU 416F-3 PN/DP failed" Do you have any idea what am I doing wrong, or is it even possible to do? Best regards, Vanja ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/25/2016 12:29:29 PMNew subject after splitting |
|
5/24/2016 9:46 PM | |
Joined: 9/8/2015 Last visit: 3/5/2024 Posts: 3 Rating: (0) |
Thanks for a fast answer. This is what I get when I try to migrate the project. |
Follow us on