3/9/2021 6:24 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
For the setpoints ON (b) and OFF (a) I would not work with the Parameter VM Mapping, but with analog network inputs. See example in the attachment.
AttachmentSetpoints.zip (426 Downloads) |
This contribution was helpful to
1 thankful Users |
3/10/2021 3:31 PM | |
Joined: 2/25/2021 Last visit: 11/2/2022 Posts: 73 Rating:
|
I see, 4 Bytes are 2 Words, so both VW4 and VW6 will be transfered to the second LOGO, right? |
3/10/2021 3:41 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
Yes, correct. VW4 = VB4 + VB5 you transfer 4 VBs with the start address VB4 = VB4 to VB7. |
3/10/2021 6:03 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
No, not for now. Can you please upload the two LOGO! Programs as ZIP files?
|
Follow us on