7/19/2016 3:04 PM | |
Joined: 9/12/2013 Last visit: 7/4/2024 Posts: 32 Rating:
|
Hello Experts, We required solution for following configuration, 1. WinCC Advanced SCADA V13 SP1. 2. Delta PLC (CPU DVP14SS211R). Delta PLC supports MODBUS RTU (RS 485) protocol, so is it possible to communicate the WinCC Advanced SCADA with Delta PLC???
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/19/2016 7:25:53 PMNew subject after splitting |
|
7/19/2016 3:55 PM | |
Joined: 6/3/2014 Last visit: 8/29/2025 Posts: 660 Rating:
|
Hello zopeparag, I found some informations in the manual and in the forum. In the WinCC Advanced manual you find the following about
I don't know if it's similar for Delta PLC MODBUS RTU, as there is no other CPU type selectable. Links in the Forum: Communication B/W Wincc flexible PC runtime and MODBUS meter?MODBUS RTU RS485 Redundancy |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
7/23/2016 9:48 AM | |
Joined: 9/12/2013 Last visit: 7/4/2024 Posts: 32 Rating:
|
Hello Experts, I have configured PC station in WInCC Advanced. And made connection using Modicon Modbus RTU driver. Also prepared a tag to read coil status and forced data from Modsim but i can not read data in Runtime. I set this for demo purpose, actually we need to read data from Delta PLC. so my questions are, 1. What device should i select while going online? 2. Which interface should i select for communication? (I have selected Com3) 3. What Access point and Interface parameter to be set in Set PG/PC interface? Kindly suggest solution at the earliest....Also please find attached backup for the reference. Thanks in advance... AttachmentProj_Backup.zip (478 Downloads) |
11/16/2016 2:02 PM | |
Joined: 2/27/2014 Last visit: 8/28/2025 Posts: 689 Rating:
|
Hello, Attached file is helpful while doing Modbus RTU communiucation in Panel/Ad Runtime. Its help of TIA portal only. Modbus RTU communication is tested with only Modicon Modbus RTU. WinCC Adv/Panle always act as Master(Modbus RTU)/Client (Modbus TCP). My suggestion would be check with modbus simulator software like Modview (Modbus Slave) to test modbus communication in WinCC Adv RT. Once it is working fine the check same Modview (Modbus Master)software with Delta PLC. If everything is working fine then try with actual WinCC and Delta communication. AttachmentModbus RTU.zip (692 Downloads) |
With Best Regards, |
|
Follow us on