12/18/2011 8:52 AM | |
Posts: 26 Rating:
|
Hi Dear all, I need some help and documents about how to communicate between wincc and cp1430 (TCP/IP) s5 plc 135u cpu922.would everyone help me? thanks |
12/19/2011 10:09 AM | |
Joined: 7/18/2011 Last visit: 4/11/2025 Posts: 521 Rating:
|
Hi Farzaneh, Here is the manual of the CP1430TCP card. In order to communicate between WinCC and S5, you'll have to configure 2 connections in the CP card. - Receive connection - Fetch passive connection If the CP card is not yet installed: -Add synchronisation blocks in start-up OB's - Add send-all/receive-all blocks in cyclic program Hope this points you a bit in the right direction. Kind regards, BV AttachmentTCP1430ke1.pdf (435 Downloads) |
Last edited by: BeVee at: 12/19/2011 10:15 AM |
|
This contribution was helpful to
1 thankful Users |
3/17/2014 4:01 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
follow up question published by winarko_songis split to a sperate thread with the subject communicate S5 115U to WinCC v7.0 using CP1430 card. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on