5/14/2021 3:04 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello Tigranes:; First, a few questions on your system: - are you sure you are using Step 7 Microwin v5.5 to program the S7-200 CPU? To my knowledge there were no versions of Microwin after v4.9 SP9... - what model number is on the PPI cable you want to use? - what is the part number of the CPU, we need to determine if it is 1st or 2nd generation, it could have an impact. - WinCC Flexible versions are distinguished by year of release and service pack, for example WinCC Flexible 2008 SP3; which version do you have? - which edition of WinCC Flexible are you using, compact, or standard (for different types of panels) or advanced runtime (for PC stations)? For the basics on connecting WinCC Flexible and a S7-200 CPU, using a PC-PPI cable look at section 3 of the pdf document available in this link:: https://support.industry.siemens.com/cs/ww/en/view/23800567 Hope this help, Daniel Chartier |
Last edited by: dchartier at: 05/14/2021 15:06:35 |
|
5/15/2021 1:37 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello tigranes; The link I provided earlier lacked the PPI cable connection information I was refering to, very sorry. Attached is the document I think you will need to setup the connection bewtween WinCC Flexible 2008 and a PC running WinCC Flex runtime. Note that the configuration is done in WinCC flexible which is the master of this connection. Study Ch. 3 of the document. Hope this helps, Daniel Chartier Attachments7-200_winccflexrt_panels_en.pdf (420 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on