5/21/2018 12:37 PM | |
Joined: 1/30/2018 Last visit: 9/20/2018 Posts: 5 Rating:
|
Hi, I would appreciate some advice on the configuration of an alarm line in a Comfort Panel using WinCC TIA v14. I have configured all my messages, some error with acknowledge and some warning with no acknowledge and would like to display the current alarm at the top of the HMI. I have been able to do this with an Alarm Line, however I have one small issue. I need to display the company logo on the top left of the screen and the time/date on the top right. I would like to fill the screen in between with the alarm, however I can find no way to adjust the width of an alarm line. Also if I set the order of alarm line to "send to back" and logo to "bring to front" this has no effect. If I configure an alarm window and resize so only the top line can be seen I can fit this into the gap and make the text large but in this case the top alarm is highlighted so does not display in the default colours unless I click away from it to deselect. I have spent quite a bit of time on this very simple issue so any help would be appreciated! Many thanks, Barry ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/22/2018 12:18:15 PMNew subject after splitting |
|
8/19/2024 2:14 PM | |
Joined: 12/11/2023 Last visit: 7/31/2025 Posts: 1 Rating:
|
Hi, you can use the "Same widht and hight option. |
Follow us on