2/21/2008 8:56 PM | |
Posts: 41 Rating: (0) |
I made it several times, before asking in the forum...Maybe something was wrong in the range settings. Thank you,Pegaia! I will chek the settings. |
2/22/2008 10:38 AM | |
Posts: 41 Rating: (0) |
Hi, Pegaia ! The project is still not working...I don't know what's wrong....I'm sending the project. The 8 subroutines have identical function. Please give me the idea where is the problem only for the first SBR , for the rest SBRs is the same.I want to conserve the actual values of the timers andcounters, the states of all bits (including timers and counters). Actually all these are included in the retentive ranges, but after power shtdown and then up all the counters are cleared... What is the project for : I need to control 12 butterfly vavles giving them time to be ON , then is a pause (another time) and how many times to repeat the cycle. In brief for the first subroutine: When I0.2 is ON the choosen values from the TD200 are transformed in minutes in network 4. Counters C0 to C4 count the minutes for the different stages of the cycle and C5 couts the number of cycles.Networks 5 to 12 are the sequence of the cycle. Do not look at the other subroutines, they still need some work... AttachmentKAMENITZA_KISNICI.zip (191 Downloads) |
2/22/2008 11:27 AM | |
Posts: 41 Rating: (0) |
Hi, Pegaia! My problems have fear of you ! After my last message with the attachment, the idea came in my head. The problem is resolved. |
2/22/2008 4:30 PM | |
Joined: 9/23/2005 Last visit: 10/18/2024 Posts: 4350 Rating: (1448) |
hi What you do to solve it? |
Denilson Pegaia |
|
Follow us on