1/11/2023 8:51 AM | |
Joined: 11/30/2020 Last visit: 8/21/2024 Posts: 10 Rating:
|
Hello; We have recently installed a new CP5623 Profibus comumunication card on Wondows 10. When we start the PC (After turning off) the CP5623 card is not found anymore either in the PG/PC interface either in the device manager (as it is shown in the images below). when we restart the PC, the driver of the card is actived and it works good, but the configuration is reset.(Example: the old DP adress was 5 and it becames 0) even if we restart the PC again (Without turning it off) the CP5623 is found with the right configuration. (The same problem apears on Windows 7.) Best regards. AttachmentCP5623 Problem.zip (563 Downloads) |
Follow us on