2/9/2023 8:46 PM | |
Joined: 4/20/2007 Last visit: 9/1/2025 Posts: 731 Rating:
|
Hi Experts! I have a CPU 1512SP F-1 PN + CP 1542SP. We use the CPU as a PROFINET controller for some drives and a RIO. As well as some MODBUS TCP devices. The CP is used for MODBUS TCP connection to SCADA. Now my client wants to add a second CP for another dedicated interface for a OPC UA server. I seem to recall that this was not possible through a CP. in a ET200SP based CPU, am I correct? Is it correct that we would need to use a full size 1500 series CPU with a CP 1543-1, and forward data. AS described in chapter 10.1 of this document? If so, would this satisfy the demand of separated networks? Thank you all! |
Follow us on