6/5/2009 6:43 PM | |
Joined: 2/16/2009 Last visit: 8/16/2025 Posts: 40 Rating:
|
Dear Members, I have one CPU 315T with Sinamics S120. My hardware configuration does not completly download after a lot of spend time. Actually i created the project and dwonload the whole project without any problem. After that i convert the X1 interface of CPU 315T from MPI to Profibus. But my hardware configuration did not download. Then i once again shift the X1 interface from Profibus to MPI. But my hardware configuration could not be download. At that moment my project Blocks download without any problem. But i face problem in download during Hardware Configuration & System Data Block. Also it does not give any error & downloading status bar stop at same position after every try. Thnaks, Best Rgards, Arif Ahmad Attachmentimg.pdf (630 Downloads) |
Extreme Control Engineering |
|
6/5/2009 7:02 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Arif, Try with memory reset, build new hardware configuration and download to CPU. Regards Hristo Mihalev |
6/6/2009 6:54 AM | |
Joined: 2/16/2009 Last visit: 8/16/2025 Posts: 40 Rating:
|
Thanks for quick response Dear Members, Dear UMENCHO & SPV: I already Clear/Reset from Hardware Config, build new hardware configuration and download to CPU.But Problem is still there. Dear Darius: I do not understand the driver problem you mention it. if driver have a problem then how to reload the driver. Thanks & Best Regards, Arif Ahmad |
Extreme Control Engineering |
|
6/6/2009 8:45 AM | |
Joined: 9/28/2005 Last visit: 7/24/2025 Posts: 2957 Rating:
|
Hello,
Usually it means to reinstall Step-7 and SIMATIC.NET is you have such. I had similar problems and it was dirvers fault. Reinstalling only Step-7 helped me back then. |
Best regards, |
|
6/7/2009 2:16 PM | |
Joined: 4/24/2008 Last visit: 1/15/2025 Posts: 213 Rating:
|
What for a speed is configurated at your ProFI/MPI Bus? |
|
|
Follow us on