11/10/2016 3:54 PM | |
Joined: 3/16/2016 Last visit: 1/16/2024 Posts: 22 Rating:
|
Dear all, I have been work in a S7_400 H redundancy system everything is working fine, but sometimes when I do a power cycle in one PLC to test the redundancy system the PLC was turn off the power when I turn on the power again is still in Stop mode and is impossible to put in RUN mode. To put again in RUN mode I need to download the hw configuration and is working again... any tip?? ------------------------------------------------------------------------------------------ AttachmentPLC_B_BUFFER.txt (552 Downloads) |
Last edited by: The Helping Hand at: 11/10/2016 6:45:17 PMNew subject after splitting |
|
11/10/2016 3:54 PM | |
Joined: 3/16/2016 Last visit: 1/16/2024 Posts: 22 Rating:
|
Sorry the PLC_A buffer too
AttachmentPLC_A_BUFFER.txt (518 Downloads) |
Follow us on